Part Number: TCA39306
Hi team,
do you see any issue when TCA39306 is being used in switch mode and customer would connect VREF2 and ENABLE to the VCC_LowTemp (3.3V) and VREF1 to VCC_HighTemp (3.3V)?
What would happen if there would be an issue if VREF2 and EN are connected to ground while VREF1 is still at 3.3V.
This would be the case when Low Temp VIO is disabled once the system reaches a certain temperature.
Is this a concern for possible back power trough on chip ESD diodes?
BR,
Stefan