Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9548A: VCC range based on the VDPUM and VDPU

Part Number: TCA9548A

Hi team,

My customer has an application for TCA9548A that I would like to ask you about:

Master side VDPUM=3.3V,

Slave side VDPU0=3.3V, VDPU1=1.8V,

Is it okay to have VCC=3.3V? If not, is it okay to have VCC=2.5V or VCC=1.8V?

  • Hey Matt,

    The Vpass(V) voltage would need to be equal or below your lowest bus voltage. So in this case you lowest  bus voltage is 1.8V. At 3.3V, the vpass on figure 14 looks like it's right at 2V. 
    At 2.5V = VDD the Vpass is about 1.5V and even less for 1.8V so these two should work fine but 3.3V wouldn't be. 

    Thanks,
    Rami