Part Number: DP83822IF
Hi,
Referring to the datasheet for DP8322IF when configured in 100Base-FX mode.
Table 7.5 shows
MDI 100BASE-FX receiver input swing requirement 0.22V to 1.8V
MDI 100BASE-FX transmitter swing 0.9V to 1.1V*
(*) with default setting.
Figure 7-20. 100BASE-FX Waveform
Shows a waveform about 0.5V peak to peak.
Q1- Is the waveform shown centered around 0V?
Q2-Is this the expected waveforms at the input to the chip in 100BaseFX mode? I.e. is this for RX?
Q3-Do you have a picture of the Transmit waveform?
Thanks
Magid