This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIOL111: Current flow different between TIOL111 and TIOL1113.

Guru 11525 points

Part Number: TIOL111

Hi team,

There is a difference in the way the current flows TIOL111 and TIOL1113 at CQpin, so I'd like to know if this is normal operation.

TIOL111 : 2A
TIOL1113 : 0.3A

Is it possible that TIOL111 is broken?
If so, what are the possible failure points?

BR,
Kengo.