Part Number: TUSB2046I
TUSB2046I is not being enumerated by the PC. I have changed the connection to RESET to a PWRGOOD connection on the LDO with a 10K pullup. I have moded the board with 10k pullups to 3.3V as well. The DP line to the upstream part now has a 15K pullup resistor but the PC is still giving a device descriptor failed message. All downstream ports are not powered I assume because the TUSB2046 has not successfully connected to the PC. Does anyone have any suggestions as to why the PC would not recognize the hub device?