Part Number: DP83867E
Other Parts Discussed in Thread: USB-2-MDIO
Hello,
My customer has the below question. Can you help us get to a resolution?
I am looking to utilize the DP83867E with SGMII and would like to use the attached TI user guide schematic reference for the phy on our board.
Before starting I wanted to be able to confirm if we can purely set the PHY only via strap resistors (no MDIO/MDC control) for 1000Mbps, full-duplex, auto negotiate and any other setting such that the interface would be plug and play?
My concern is that currently we have an implementation of DP83867E but with RGMII and MDIO access although it is not plug and play. Meaning that currently we need to send via MDIO to change the PHYCR Force_link_good to 0 so that we can get the port to link up.
I wanted to be able to confirm if Force_link_good bit 10 in PHYCR is something that needs to be set for SGMII interface mode as well? And if so, can I set PHYCR bit 10 to 0 via strap resistors such that we can achieve a configured PHY without using MDIO/MDC?
Alternatives
- Open to hearing any possible alternatives of a similarly spec’d PHY that can be assuredly a plug and play PHY via strap resistors only.
- If MDIO is not accessible can JTAG be used to configure the PHY register?
Thanks for the help!
Best,
Adam