Part Number: TPD1S414
Other Parts Discussed in Thread: TVS2200, TVS1800, , TPD1S514
Tool/software:
I have a customer designing a high volume product with USBC, but only 5V VBUS (no PD). They would like to protect against the case of a non-compliant USBC cable that presents a hot 20V to the system. The downstream components have an absmax of 26V, and surge testing has shown spikes exceeding 26V.
My question:
- TVS2200 is the one I normally think of first for USBC VBUS, but it doesnt clamp until beyond 26V so in this case it wont work.
- TVS1800 seems to clamp near 20-21V, so I worry a hot 20Vdc cable would just burn this thing up.
you agree with those two statements? Is the TPD1S414 the best device for this condition?
Thanks,
Brian