Part Number: SN65DP159
Tool/software:
Dear Specialists,
My customer is considering SN65DP159 and has a question.
I would be grateful if you could advise.
---
Regarding SN65DP159,
DatasheetP.20 9.3.2 Operation Timing
There are two regulations listed below regarding VCC/VDD startup.
① VCC/VDD startup timing difference is 200us or less
② VCC/VDD ramp-up time is 100ms or less
listed above, in order to suppress the inrush current, set ② as close to 100ms as possible.
I would like to design it, but then it would be difficult to follow ①.
(Since it is 200us for 100ms, the relative value is very small.)
Could you please let me know if there are any harms caused by not observing ①?
---
I appreciate your great help in advance.
Best regards,
Shinichi