Part Number: DP83848K
Tool/software:
May I ask why the temporary register " False Carrier Sense Latch " becomes high? Will this temporary register becoming high cause the connection to be disconnected?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Joe,
This happens when there is an error in the incoming data. This should not cause a link down on it's own. Link can be checked by reading Register 0x1.

Taken from Page 44 of DP83848x data sheet
Regards,
Alvaro
Hi Joe,
This is correct. However if you are having link down issues, this would give us a hint as to what the root cause is. What is current problem that you are facing? Are we losing link unexpectedly? Could you provide more information?
Regards,
Alvaro
We are currently experiencing a sudden disconnection when using the DP83848K PHY for a period of time, but sometimes it is always normal. Currently, it is found that the disconnection is caused by an error received by the DP83848K PHY. Is there any debug message for the DP83848K PHY to assist in further analysis?Hi Joe,
Questions:
For further debug, read all registers during a working case, then during non-working and see what changed. Is this what you already did and "False Carrier Sense" was the only register that changed?
Regards,
Alvaro
Hi Alvaro:
Reply is as follows
Ans:The connection will be automatically restored without restarting, and sometimes the disconnection problem will not occur after the connection is restored. The disconnection problem occurs randomly.
2.Does this happen when we use a different cable or different link partners?
Ans:I have replaced peripheral equipment and cables, but the problem still exists.
3.What is the current test procedure?
Ans:Our machine operates at low temperatures of -40 degrees Celsius
4.How long is the link stable before dropping link?
Ans:Restores the connection in about 30 seconds after being disconnected
5.What speed if the PHY linking up at?
Ans:The connection is made at a speed of 100M
For further debug, read all registers during a working case, then during non-working and see what changed. Is this what you already did and "False Carrier Sense" was the only register that changed?
Ans:When a network disconnection occurs, the Debug message displayed on the SOC indicates that the PHY is disconnected, and the "False Carrier Sense" register will definitely become High. However, if "False Carrier Sense" becomes High, the disconnection may not occur.
Currently, judging from the SOC message, I don't know why the PHY and SOC lost connection when the network was disconnected.
Thanks
Joeyan
Hi Joe,
Our machine operates at low temperatures of -40 degrees Celsius
Thank you for mentioning this. Is it possible to run this test at room temperate (25C)? I want to rule out the possibility of this being temperature dependent.
As for Reg 0x1, this change is to be expected. It tells us that the link is down, auto-negotiation is a mechanism used to establish link, so if link goes down then then auto-neg status is also expected to go down.
Reg 0x14 in your Link Fail log shows the maximum amount of RX Errors, this could be the reason of the link down. Is the link partner also at -40C?
Regards,
Alvaro
Hi Alvaro:
1、Thank you for mentioning this. Is it possible to run this test at room temperate (25C)? I want to rule out the possibility of this being temperature dependent.
Ans: Our Camera works at -40 degrees, but the IC works at around 10 degrees (there is a heater inside the camera)
2、As for Reg 0x1, this change is to be expected. It tells us that the link is down, auto-negotiation is a mechanism used to establish link, so if link goes down then then auto-neg status is also expected to go down.
Ans:We can judge from this that the SOC and PHY are connected normally, but is there a problem with the connection between the PHY and the external Hub?
3、Reg 0x14 in your Link Fail log shows the maximum amount of RX Errors, this could be the reason of the link down. Is the link partner also at -40C?
Ans:Except for our machine, which is in the chamber at -40 degrees, the rest of our equipment is in an outdoor environment of 25 degrees.
Thanks
Joeyan
Hi Joeyan,
Did you try the test setup with the board outside of the -40 degree chamber? Do we still see the same issues?
Regards,
Alvaro
Because the problem occurs randomly, sometimes the problem persists at a low temperature of -40°C,
and sometimes it has not been disconnected for four days.
In addition, the temporary register information I provided last time can be judged to be that the SOC and PHY are normal.
Is there a problem with the external Hub section of the PHY? Are there other registers that can help with further judgment?Hi Joe,
This is difficult for me to debug. The False carrier sense latch message could be a hint about the connector side signal getting corrupted. Is the transformer and all other components on your board rated for -40C too? Again I would try to reproduce this at room temperature and in many different ways to try to consistently recreate this issue.
When the link goes down, you mentioned that sometimes the link will come back on it's own, without the need to power-cycle, unplug the cable, or restart auto-negotiation. How long is the link down when this issue arises?
Regards,
Alvaro
The disconnection time is very random, sometimes it lasts for 30 seconds, and sometimes it keeps disconnecting and reconnecting
repeatedly, but in the end it will automatically restore the connection. Is there a way for DP83848K to further confirm?Hi Joe,
Could we try different cable lengths? I can try to recreate this issue in lab (at room temperature) and get back to you next week.
Regards,
Alvaro