Part Number: LMH0318
Tool/software:
I get only 700 mV of amplitude on OUT0 instead of 800 mV as expected.
When reading the OUT0_VOD register (0x80) I get 0x20 instead of the default value 0x54.
0x20 is not an expected value because this is an invalid value for bit 7-4 and the reserved bit 2 is not set.

By modifying this value, I get also 700 mV with the 0x54 value. I must set 0x50 to get the expected 800 mV of amplitude.
What is wrong ? Why I didn't get the 800 mV by default? Must the bit 2 be set or clear. Which value should I set to this register?
Regards
Jean-François