Tool/software:
hello! We use DSI-> RGB888---->DS90UB681------FPD link III-------DS90UB940------YUV422 ->CSI, Can you provide a register configuration table for UB940.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
hello! We use DSI-> RGB888---->DS90UB681------FPD link III-------DS90UB940------YUV422 ->CSI, Can you provide a register configuration table for UB940.
Hi Lin,
I have attached the register writes to configure the 940 as you described. Do you need CSI continuous clock or the VCID to be set to a particular value?
Best,
Jack
desAddr = 0x58 board.WriteI2C(desAddr, 0x2, 0x80) #Disable video output board.WriteI2C(desAddr, 0x6A, 0x20) #CSI 2 lanes, non-continuous clock board.WriteI2C(desAddr, 0x6B, 0x50) #Input data RGB444, output CSI YUV422_8 board.WriteI2C(desAddr, 0x2, 0x90) #Enable video output
Hi Lin,
I modified the code for CSI continuous clock. The VCID is set to 0 by default so there are no register writes needed.
Best,
Jack
desAddr = 0x58 board.WriteI2C(desAddr, 0x2, 0x80) #Disable video output board.WriteI2C(desAddr, 0x6A, 0x22) #CSI 2 lanes, continuous clock board.WriteI2C(desAddr, 0x6B, 0x50) #Input data RGB444, output CSI YUV422_8 board.WriteI2C(desAddr, 0x2, 0x90) #Enable video output