Part Number: DP83867IR
Tool/software:
Dear Team
I would like to design a circuit using the "DP83867IRPAPR" PHY.
[RJ45 - Lan Trans - PHY - SOC ]
The BD is designed separately from [RJ45-LAN TRANS] and [SOC], and the two BDs are connected with a cable.
Total Ethernet Legnth is the same, but MDI / MII Length varies depending on PHY placement
If the PHY is placed on the [RJ45-LAN TRANS] BD, the MDI analog signal will be shortened, which seems to be advantageous for EMC.
However, there are many PHY signals that must be connected to the SOC with cables, and the connector area is likely to be weak to EMC.
On the other hand, if the PHY is placed in the [SOC] BD, the MDI analog signal becomes longer, which is likely to be disadvantageous to EMC.
However, since the only signal connected to the Lan Transformer is the MDI Line, signal loss at the connector is likely to be minimal.
Through www.ti.com/.../snla387.pdf, MDI Max Trace was confirmed to be 2000 mils and MII Max Trace was confirmed to be 6000 mils.
There will be no problem with communication, but it seems important to keep the MDI signal short in terms of EMC, but I am not sure.
Please let me know your thoughts.
Thank you.