This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB522P: TI# TUSB522PIRGET Technical issue

Part Number: TUSB522P

Tool/software:

We are currently encountering a problem with the TI model TUSB522PIRGET when making cables. Please help us answer the reason and protocol requirements. thanks
The cable has three interfaces: Type C female, Type C male, and DC 12V input
block diagram
1:DC input 12V,  DCDC convert to 3.3V to supply power to TUSB522P
2: USB 3.0 extended through TUSB522P
       USB 2.0 Direct Link
 
Problem points:
There is  an issue with the order of interface insertion, there may be device unrecognized issues when the DC head is inserted last
Type-C Female Type-C male DC 12V  input find USB3.0 device 
1
2 3 No
1 3 2 Yes
  1,2,3:  These numbers refer to the order of interface insertion