This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550-Q1: CAN transceiver send/recewive message

Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550

Tool/software:

Hello,

I completed the TCAN4550 initialization refer to  the TCAN demo, but when I called the function 

TCAN4x5x_MCAN_ClearInterruptsAll     // Resets all MCAN interrupts (does NOT include any SPIERR interrupts).

then I call TCAN4x5x_MCAN_WriteTXBuffer to write to the TxBuffer,  I received a CANERR from TCAN with SPI communication.

the Log as  follows (W and R are synchronous) :

ClearInterruptsAll
W: 0x61 0x10 0x50 0x01 0xff 0xff 0xff 0xff
R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
W: 0x61 0x81 0x74 0x04
R: 0xa0 0x00 0x00 0x00

Regards,

Leon

  • Hello Leon,

    The Global Status Byte returned on your SPI write is 0xA0 which shows the CAN Error (CANERR) bit is getting set.  This is the Logical OR of the CAN Silent (CANSLNT) and the CAN Stuck Dominant (CANDOM) bits in the Interrupts register 0x0820.  You should read this register to determine which bit is responsible for setting the CANERR flag.

    Note that the CANSLNT bit will be set if there is no CAN activity (recessive to dominant transitions) for longer than approximately 1 second.

    I'm not sure if you are just providing me some of the SPI R/W information to ask about the CANERR, but the second write you have provide shows a Length field of 4 words, but there is not any data.  For a Length field of 4, you should have an additional 16 bytes of data in the write and read.

    Regards,

    Jonathan

  • Hi Jonathan

    I`m sorry, I didn't express myself fully. After  called  the function Init_CAN, I followed the TCAN demo as shown in the figure: 

    and the register 0x0820 show data (R: 0x00 0x00 0x04 0xa0), It is CANSLNT. 

    ClearInterruptsAll
    W: 0x61 0x10 0x50 0x01 0xff 0xff 0xff 0xff
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
    W: 0x61 0x81 0x74 0x04
    R: 0xa0 0x00 0x00 0x00
    W: 0x05 0x10 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    W: 0x00 0x38 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    W: 0x88 0x77 0x66 0x55
    R: 0x00 0x00 0x00 0x00
    W: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    W: 0x41 0x08 0x20 0x01
    R: 0xa0 0x00 0x00 0x00
    R: 0x00 0x00 0x04 0xa0
    W: 0x61 0x81 0xbc 0x06
    R: 0xa0 0x00 0x00 0x00
    W: 0x04 0x8c 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    W: 0x00 0x3a 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    W: 0x44 0x33 0x22 0x11
    R: 0x00 0x00 0x00 0x00
    W: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    W: 0x00 0x00 0x01 0x23
    R: 0x00 0x00 0x00 0x00
    W: 0x00 0x00 0x00 0x3a
    R: 0x00 0x00 0x00 0x00
    W: 0x61 0x10 0xd0 0x01 0x00 0x00 0x00 0x02
    R: 0xa0 0x00 0x00 0x00 0x00 0x00 0x00 0x00
    W: 0x61 0x10 0xd0 0x01 0x00 0x00 0x00 0x01
    R: 0xa0 0x00 0x00 0x00 0x00 0x00 0x00 0x00

    and CANOE receive frame as follow:

  • and the register 0x0830 showed CANSLNT is disabled when I writed Tx Buffer.

    W: 0x41 0x08 0x30 0x01
    R: 0xa0 0x00 0x00 0x00

  • Hi Leon,

    The CANSLNT bit will get set if there is no CAN activity within approximately 1 second which may be an indication of an error such as broken or cut wires, etc.  Once activity resumes, the bit should be cleared.

    The Stuff error could come from a difference in the bit timing configuration between the TCAN4550 and the CANoe settings.  Please verify that the settings of the TCAN4550 match those of the CANoe configuration.  Also, make sure there is not some other physical issue with the bus and that there are termination resistors at both ends.  The bus should have a total of 60ohms of resistance between CANH and CANL.

    If the bit timing and sampling position settings are different, or there is some sort of issue with the CAN bus degrading the signal integrity, then there could be sampling issues.

    But a Stuff error is when 6 or more bits are detected of the same value which is not allowed per the protocol.  The Data array in the code should prevent this, or the device should automatically insert a stuff bit if needed.  So if the device is working correctly, and the bit timings are ok, then an additional bit should be inserted to prevent this error if the data had 6 or more consecutive 1's or 0's.

    Can you capture the CANH and CANL waveforms so we can see what is being produced by the device when you transmit a message?

    Regards,

    Jonathan

  • Hi Jonathan

    I used an oscilloscope to measure the voltage range of CANL and CANH when I transmited a message, the CANL and CANH are 2.0- 2.8v.

    I writed Tx Buffer as follow:

    I capture the CANH and CANL waveforms by Logic analysis. But the data are very strange. It's almost always 1

    The CAN frame decoder:

    Id,Time[ns],CAN-FD: Fields
    1,49999920.00,Start of frame
    2,50001920.00,Identifier: 0 (0x0)
    3,50023920.00,Remote transmission request: data frame
    4,50025920.00,Identifier extension bit: standard frame
    5,50027920.00,Flexible data format: 0
    6,50029920.00,Data length code: 0
    7,50037920.00,CRC-15 sequence: 0x0000
    8,50067920.00,CRC delimiter: 0
    9,50069920.00,ACK slot: ACK
    10,50071920.00,ACK delimiter: 0
    11,50073920.00,End of frame
    12,1231798240.00,Start of frame
    13,1231800240.00,Identifier: 2047 (0x7ff)
    14,1231822240.00,Substitute remote request: 1
    15,1231824240.00,Identifier extension bit: extended frame
    16,1231826240.00,Extended Identifier: 262143 (0x3ffff)
    17,1231826240.00,Full Identifier: 536870911 (0x1fffffff)
    18,1231862240.00,Remote requset substituion: 1
    19,1231864240.00,Flexible data format: 1
    20,1231866240.00,Reserved bit 0: 1
    21,1231869440.00,Bit rate switch: 1
    22,1231870320.00,Error state indicator: 1
    23,1231870840.00,Data length code: 15
    24,1231872840.00,Data byte 0: 0xff
    25,1231876840.00,Data byte 1: 0xff
    26,1231880840.00,Data byte 2: 0xff
    27,1231884840.00,Data byte 3: 0xff
    28,1231888840.00,Data byte 4: 0xff
    29,1231892840.00,Data byte 5: 0xff
    30,1231896840.00,Data byte 6: 0xff
    31,1231900840.00,Data byte 7: 0xff
    32,1231904840.00,Data byte 8: 0xff
    33,1231908840.00,Data byte 9: 0xff
    34,1231912840.00,Data byte 10: 0xff
    35,1231916840.00,Data byte 11: 0xff
    36,1231920840.00,Data byte 12: 0xff
    37,1231924840.00,Data byte 13: 0xff
    38,1231928840.00,Data byte 14: 0xff
    39,1231932840.00,Data byte 15: 0xff
    40,1231936840.00,Data byte 16: 0xff
    41,1231940840.00,Data byte 17: 0xff
    42,1231944840.00,Data byte 18: 0xff
    43,1231948840.00,Data byte 19: 0xff
    44,1231952840.00,Data byte 20: 0xff
    45,1231956840.00,Data byte 21: 0xff
    46,1231960840.00,Data byte 22: 0xff
    47,1231964840.00,Data byte 23: 0xff
    48,1231968840.00,Data byte 24: 0xff
    49,1231972840.00,Data byte 25: 0xff
    50,1231976840.00,Data byte 26: 0xff
    51,1231980840.00,Data byte 27: 0xff
    52,1231984840.00,Data byte 28: 0xff
    53,1231988840.00,Data byte 29: 0xff
    54,1231992840.00,Data byte 30: 0xff
    55,1231996840.00,Data byte 31: 0xff
    56,1232000840.00,Data byte 32: 0xff
    57,1232004840.00,Data byte 33: 0xff
    58,1232008840.00,Data byte 34: 0xff
    59,1232012840.00,Data byte 35: 0xff
    60,1232016840.00,Data byte 36: 0xff
    61,1232020840.00,Data byte 37: 0xff
    62,1232024840.00,Data byte 38: 0xff
    63,1232028840.00,Data byte 39: 0xff
    64,1232032840.00,Data byte 40: 0xff
    65,1232036840.00,Data byte 41: 0xff
    66,1232040840.00,Data byte 42: 0xff
    67,1232044840.00,Data byte 43: 0xff
    68,1232048840.00,Data byte 44: 0xff
    69,1232052840.00,Data byte 45: 0xff
    70,1232056840.00,Data byte 46: 0xff
    71,1232060840.00,Data byte 47: 0xff
    72,1232064840.00,Data byte 48: 0xff
    73,1232068840.00,Data byte 49: 0xff
    74,1232072840.00,Data byte 50: 0xff
    75,1232076840.00,Data byte 51: 0xff
    76,1232080840.00,Data byte 52: 0xff
    77,1232084840.00,Data byte 53: 0xff
    78,1232088840.00,Data byte 54: 0xff
    79,1232092840.00,Data byte 55: 0xff
    80,1232096840.00,Data byte 56: 0xff
    81,1232100840.00,Data byte 57: 0xff
    82,1232104840.00,Data byte 58: 0xff
    83,1232108840.00,Data byte 59: 0xff
    84,1232112840.00,Data byte 60: 0xff
    85,1232116840.00,Data byte 61: 0xff
    86,1232120840.00,Data byte 62: 0xff
    87,1232124840.00,Data byte 63: 0xff
    88,1232129320.00,Stuff count: 111
    89,1232130840.00,Parity: 1
    90,1232131320.00,CRC-21 sequence: 0x1fffff
    91,1232144840.00,CRC delimiter: 1
    92,1232971840.00,ACK slot: NACK
    93,1232973840.00,ACK delimiter: 1
    94,1232975840.00,End of frame
    95,1233089640.00,Start of frame
    96,1233091640.00,Identifier: 0 (0x0)
    97,1233113640.00,Remote transmission request: data frame
    98,1233115640.00,Identifier extension bit: standard frame
    99,1233117640.00,Flexible data format: 0
    100,1233119640.00,Data length code: 3
    101,1233129640.00,Data byte 0: 0xff
    102,1233145640.00,Data byte 1: 0xff
    103,1233161640.00,Data byte 2: 0xff
    104,1233179640.00,CRC-15 sequence: 0x7fff
    105,1233209640.00,CRC delimiter: 1
    106,1233211640.00,ACK slot: NACK
    107,1233213640.00,ACK delimiter: 1
    108,1233215640.00,End of frame
    109,1233277640.00,Start of frame
    110,1233279640.00,Identifier: 2047 (0x7ff)
    111,1233301640.00,Substitute remote request: 1
    112,1233303640.00,Identifier extension bit: extended frame
    113,1233305640.00,Extended Identifier: 262143 (0x3ffff)
    114,1233305640.00,Full Identifier: 536870911 (0x1fffffff)
    115,1233343640.00,Remote requset substituion: 1
    116,1233345640.00,Flexible data format: 1
    117,1233347640.00,Reserved bit 0: 1
    118,1233350840.00,Bit rate switch: 1
    119,1233351720.00,Error state indicator: 1
    120,1233352240.00,Data length code: 15
    121,1233354240.00,Data byte 0: 0xff
    122,1233358240.00,Data byte 1: 0xff
    123,1233362240.00,Data byte 2: 0xff
    124,1233366240.00,Data byte 3: 0xff
    125,1233370240.00,Data byte 4: 0xff
    126,1233374240.00,Data byte 5: 0xff
    127,1233378240.00,Data byte 6: 0xfc
    128,1233383120.00,Data byte 7: 0x7f
    129,1233387120.00,Data byte 8: 0xff
    130,1233391120.00,Data byte 9: 0xff
    131,1233395120.00,Data byte 10: 0xff
    132,1233399120.00,Data byte 11: 0xff
    133,1233403120.00,Data byte 12: 0xff
    134,1233407120.00,Data byte 13: 0xff
    135,1233411120.00,Data byte 14: 0xff
    136,1233415120.00,Data byte 15: 0xff
    137,1233419120.00,Data byte 16: 0xff
    138,1233423120.00,Data byte 17: 0xff
    139,1233427120.00,Data byte 18: 0xff
    140,1233431120.00,Data byte 19: 0xf8
    141,1233435640.00,Data byte 20: 0xff
    142,1233439640.00,Data byte 21: 0xff
    143,1233443640.00,Data byte 22: 0xff
    144,1233447640.00,Data byte 23: 0xff
    145,1233451640.00,Data byte 24: 0xff
    146,1233455640.00,Data byte 25: 0xff
    147,1233459640.00,Data byte 26: 0xff
    148,1233463640.00,Data byte 27: 0xff
    149,1233467640.00,Data byte 28: 0xff
    150,1233471640.00,Data byte 29: 0xff
    151,1233475640.00,Data byte 30: 0xff
    152,1233479640.00,Data byte 31: 0xff
    153,1233483640.00,Data byte 32: 0xf1
    154,1233488120.00,Data byte 33: 0xff
    155,1233492120.00,Data byte 34: 0xff
    156,1233496120.00,Data byte 35: 0xff
    157,1233500120.00,Data byte 36: 0xff
    158,1233504120.00,Data byte 37: 0xff
    159,1233508120.00,Data byte 38: 0xff
    160,1233512120.00,Data byte 39: 0xff
    161,1233516120.00,Data byte 40: 0xff
    162,1233520120.00,Data byte 41: 0xff
    163,1233524120.00,Data byte 42: 0xff
    164,1233528120.00,Data byte 43: 0xff
    165,1233532120.00,Data byte 44: 0xff
    166,1233536120.00,Data byte 45: 0xe3
    167,1233540640.00,Data byte 46: 0xff
    168,1233544640.00,Data byte 47: 0xff
    169,1233548640.00,Data byte 48: 0xff
    170,1233552640.00,Data byte 49: 0xff
    171,1233556640.00,Data byte 50: 0xff
    172,1233560640.00,Data byte 51: 0xff
    173,1233564640.00,Data byte 52: 0xff
    174,1233568640.00,Data byte 53: 0xff
    175,1233572640.00,Data byte 54: 0xff
    176,1233576640.00,Data byte 55: 0xff
    177,1233580640.00,Data byte 56: 0xff
    178,1233584640.00,Data byte 57: 0xff
    179,1233588640.00,Data byte 58: 0xc7
    180,1233593120.00,Data byte 59: 0xff
    181,1233597120.00,Data byte 60: 0xff
    182,1233601120.00,Data byte 61: 0xff
    183,1233605120.00,Data byte 62: 0xff
    184,1233609120.00,Data byte 63: 0xff
    185,1233613640.00,Stuff count: 111
    186,1233615120.00,Parity: 1
    187,1233615600.00,CRC-21 sequence: 0x1fffff
    188,1233629120.00,CRC delimiter: 1
    189,1233641640.00,ACK slot: ACK
    190,1233643640.00,ACK delimiter: 1
    191,1233645640.00,End of frame
    192,1233693680.00,Start of frame
    193,1233695680.00,Identifier: 2047 (0x7ff)
    194,1233717680.00,Substitute remote request: 1
    195,1233719680.00,Identifier extension bit: extended frame
    196,1233721680.00,Extended Identifier: 262143 (0x3ffff)
    197,1233721680.00,Full Identifier: 536870911 (0x1fffffff)
    198,1233759680.00,Remote requset substituion: 1
    199,1233761680.00,Flexible data format: 1
    200,1233763680.00,Reserved bit 0: 1
    201,1233766880.00,Bit rate switch: 1
    202,1233767760.00,Error state indicator: 1
    203,1233768280.00,Data length code: 15
    204,1233770280.00,Data byte 0: 0xff
    205,1233774280.00,Data byte 1: 0xff
    206,1233778280.00,Data byte 2: 0xff
    207,1233782280.00,Data byte 3: 0xff
    208,1233786280.00,Data byte 4: 0xff
    209,1233790280.00,Data byte 5: 0xff
    210,1233794280.00,Data byte 6: 0xfc
    211,1233799160.00,Data byte 7: 0x7f
    212,1233803160.00,Data byte 8: 0xff
    213,1233807160.00,Data byte 9: 0xff
    214,1233811160.00,Data byte 10: 0xff
    215,1233815160.00,Data byte 11: 0xff
    216,1233819160.00,Data byte 12: 0xff
    217,1233823160.00,Data byte 13: 0xff
    218,1233827160.00,Data byte 14: 0xff
    219,1233831160.00,Data byte 15: 0xff
    220,1233835160.00,Data byte 16: 0xff
    221,1233839160.00,Data byte 17: 0xff
    222,1233843160.00,Data byte 18: 0xff
    223,1233847160.00,Data byte 19: 0xf8
    224,1233851680.00,Data byte 20: 0xff
    225,1233855680.00,Data byte 21: 0xff
    226,1233859680.00,Data byte 22: 0xff
    227,1233863680.00,Data byte 23: 0xff
    228,1233867680.00,Data byte 24: 0xff
    229,1233871680.00,Data byte 25: 0xff
    230,1233875680.00,Data byte 26: 0xff
    231,1233879680.00,Data byte 27: 0xff
    232,1233883680.00,Data byte 28: 0xff
    233,1233887680.00,Data byte 29: 0xff
    234,1233891680.00,Data byte 30: 0xff
    235,1233895680.00,Data byte 31: 0xff
    236,1233899680.00,Data byte 32: 0xf3
    237,1233904160.00,Data byte 33: 0xff
    238,1233908160.00,Data byte 34: 0xff
    239,1233912160.00,Data byte 35: 0xff
    240,1233916160.00,Data byte 36: 0xff
    241,1233920160.00,Data byte 37: 0xff
    242,1233924160.00,Data byte 38: 0xff
    243,1233928160.00,Data byte 39: 0xff
    244,1233932160.00,Data byte 40: 0xff
    245,1233936160.00,Data byte 41: 0xff
    246,1233940160.00,Data byte 42: 0xff
    247,1233944160.00,Data byte 43: 0xff
    248,1233948160.00,Data byte 44: 0xff
    249,1233952160.00,Data byte 45: 0xff
    250,1233956160.00,Data byte 46: 0xff
    251,1233960160.00,Data byte 47: 0xff
    252,1233964160.00,Data byte 48: 0xff
    253,1233968160.00,Data byte 49: 0xff
    254,1233972160.00,Data byte 50: 0xff
    255,1233976160.00,Data byte 51: 0xff
    256,1233980160.00,Data byte 52: 0xff
    257,1233984160.00,Data byte 53: 0xff
    258,1233988160.00,Data byte 54: 0xff
    259,1233992160.00,Data byte 55: 0xff
    260,1233996160.00,Data byte 56: 0xff
    261,1234000160.00,Data byte 57: 0xff
    262,1234004160.00,Data byte 58: 0xff
    263,1234008160.00,Data byte 59: 0xff
    264,1234012160.00,Data byte 60: 0xff
    265,1234016160.00,Data byte 61: 0xff
    266,1234020160.00,Data byte 62: 0xff
    267,1234024160.00,Data byte 63: 0xff
    268,1234028680.00,Stuff count: 111
    269,1234030160.00,Parity: 1
    270,1234030640.00,CRC-21 sequence: 0x1fffff
    271,1234044160.00,CRC delimiter: 1
    272,1234473680.00,ACK slot: NACK
    273,1234475680.00,ACK delimiter: 1
    274,1234477680.00,End of frame
    

  • error corrected: I used an oscilloscope to measure the voltage range of CANL and CANH when I transmited a message, the CANL and CANH are 2.0- 2.8v.

    the CANL and CANH are 2.0- 2.8v. It is the voltage after powering on, not  transmite messages.

    when I transmited a message, oscilloscope  capture the CANH and CANL waveforms as follow:

  • Hi Leon,

    Can you provide me a register dump (read back value) of all the register values your code is configuring the TCAN4550 with so that I can review the final device configuration?

    Are you trying to send data payloads with all 0xFF bytes?  The data buffer array in the demo code does not have 0xFF bytes, nor does it transmit 64 byte frames, so I wanted to verify what you expect the CAN message to be?  Can you read back the contents of the TX Message Buffer before you send it so that we can compare that to what you think you are trying to send?

    What are the bytes in the TX buffer for the message you are trying to transmit?  I would like to confirm all of the bits are correct.

    If there is a difference in any of the TX buffer contents, then we may not be transmitting a valid CAN frame, or we may have an address issue and are trying to send a message from an different TX buffer.

    Another good debug tool would be to use a logic analyzer to capture the SPI read and write communication into a log.

    Regards,

    Jonathan

  • Hi Jonathan,

    1.You can review the final device configuration by file_log.txt.   

    2. I am  not   trying to send data payloads with all 0xFF bytes, I am trying two msgs:

        uint8_t data[8] = {0x55, 0x66, 0x77, 0x88};     // Define the data payload
        header.DLC = MCAN_DLC_8B;                       // Set the DLC to be equal to or less than the data payload (it is ok to pass a 64 byte data array into the WriteTXFIFO function if your DLC is 8 bytes, only the first 8 bytes will be read)
        header.ID = 0x144;                              // Set the ID
        header.FDF = 1;                                 // CAN FD frame enabled
        header.BRS = 1;                                 // Bit rate switch enabled
        
            /* Let's make a different CAN message */
        data[0] = 0x11;
        data[1] = 0x22;
        data[2] = 0x33;
        data[3] = 0x44;                                 // Define the data payload
        header.DLC = MCAN_DLC_16B;                       // Set the DLC to be equal to or less than the data payload (it is ok to pass a 64 byte data array into the WriteTXFIFO function if your DLC is 8 bytes, only the first 8 bytes will be read)
        header.ID = 0x123;                              // Set the ID
        header.FDF = 1;                                 // CAN FD frame enabled
        header.BRS = 1;                                 // Bit rate switch enabled
        header.EFC = 0;
        header.MM  = 0;
        header.RTR = 0;
        header.XTD = 0;                                 // We are not using an extended ID in this example
        header.ESI = 0;                                 // Error state indicator

    3. the contents of the TX Message Buffer before you send it :  

    W: 0x41 0x81 0x74 0x24

    TX buffer Data,star address:0x8174
    R: 0xa0 0x00 0x00 0x00
    R: 0x05 0x10 0x00 0x00
    R: 0x00 0x38 0x00 0x00
    R: 0x88 0x77 0x66 0x55
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x04 0x8c 0x00 0x00
    R: 0x00 0x3a 0x00 0x00
    R: 0x44 0x33 0x22 0x11
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x01 0x23
    R: 0x00 0x00 0x00 0x3a
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00
    R: 0x00 0x00 0x00 0x00

     

    The MRAM confihuration:

    [TCAN] TCAN4550 Test Started...
    
    TCAN4x5x_Device_ClearSPIERR & Disable all non-MCAN Interrupt
    W: 0x61 0x00 0x0c 0x01 0xff 0xff 0xff 0xff 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x61 0x08 0x30 0x01 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x08 0x30 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x80 0x96 0x28 0xff 
    W: 0x41 0x08 0x20 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x10 0x00 0x00 
    
    If the Power On ,clear it.
    W: 0x61 0x08 0x20 0x01 0x00 0x10 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x18 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x19 
    
    W: 0x61 0x10 0x18 0x01 0x00 0x00 0x00 0x03 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x18 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x1b 
    
    TCAN4x5x_MCAN_EnableProtectedRegisters
    W: 0x61 0x10 0x18 0x01 0x00 0x00 0x03 0x03 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x18 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x03 0x1b 
    W: 0x41 0x08 0x00 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0xc8 0x00 0x04 0x68 
    
    GlobalFilter
    W: 0x61 0x10 0x80 0x01 0x00 0x00 0x00 0x03 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x80 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x03 
    
    NominalTiming_Simple
    W: 0x61 0x10 0x1c 0x01 0x0e 0x01 0x1e 0x07 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x1c 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x0e 0x01 0x1e 0x07 
    
    DataTiming_Simple
    W: 0x61 0x10 0x0c 0x01 0x00 0x80 0x0d 0x44 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x0c 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x80 0x0d 0x44 
    W: 0x61 0x10 0x48 0x01 0x00 0x00 0x0e 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x48 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x0e 0x00 
    W: 0x61 0x10 0x20 0x01 0x00 0x00 0x00 0x02 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    
    TCAN4x5x_MRAM_Clear
    W: 0x61 0x80 0x00 0x01 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    ...
    W: 0x61 0x87 0xf8 0x01 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x61 0x87 0xfc 0x01 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    
    MRAMConfiguration
    W: 0x61 0x10 0x84 0x01 0x00 0x01 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x84 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x01 0x00 0x00 
    W: 0x61 0x10 0x88 0x01 0x00 0x01 0x00 0x04 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x88 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x01 0x00 0x04 
    W: 0x61 0x10 0xa0 0x01 0x80 0x05 0x00 0x0c 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0xa0 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x80 0x05 0x00 0x0c 
    W: 0x61 0x10 0xb0 0x01 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0xb0 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    W: 0x61 0x10 0xac 0x01 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0xac 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    W: 0x61 0x10 0xf0 0x01 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0xf0 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    W: 0x61 0x10 0xc0 0x01 0x42 0x00 0x01 0x74 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0xc0 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x42 0x00 0x01 0x74 
    W: 0x61 0x10 0xbc 0x01 0x00 0x00 0x07 0x77 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0xbc 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x07 0x77 
    W: 0x61 0x10 0xc8 0x01 0x00 0x00 0x00 0x07 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0xc8 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x07 
    
    DisableProtectedRegisters
    W: 0x41 0x10 0x18 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x03 0x1b 
    W: 0x61 0x10 0x18 0x01 0x00 0x00 0x03 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x10 0x18 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x03 0x19 
    W: 0x61 0x10 0x54 0x01 0x00 0x00 0x00 0x01 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x61 0x10 0x5c 0x01 0x00 0x00 0x00 0x01 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x61 0x80 0x00 0x01 0xa8 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x80 0x00 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0xa8 0x00 0x00 0x00 
    W: 0x61 0x80 0x04 0x01 0xb2 0x34 0x56 0x78 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x80 0x04 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0xb2 0x34 0x56 0x78 
    W: 0x61 0x80 0x08 0x01 0x9f 0xff 0xff 0xff 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x80 0x08 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x9f 0xff 0xff 0xff 
    
    Device_Configure
    W: 0x41 0x08 0x00 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0xc8 0x00 0x04 0x68 
    W: 0x61 0x08 0x00 0x01 0xc8 0x00 0x04 0x60 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x08 0x00 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0xc8 0x00 0x04 0x60 
    
    Device_SetMode
    W: 0x41 0x08 0x00 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0xc8 0x00 0x04 0x60 
    W: 0x61 0x08 0x00 0x01 0xc8 0x00 0x04 0xa0 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x08 0x00 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0xc8 0x00 0x04 0xa0 
    
    ClearInterruptsAll
    W: 0x61 0x10 0x50 0x01 0xff 0xff 0xff 0xff 
    R: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x41 0x08 0x30 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x80 0x96 0x28 0xff 
    
    write tx buffer
    W: 0x61 0x81 0x74 0x04 
    R: 0xa0 0x00 0x00 0x00 
    W: 0x05 0x10 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    W: 0x00 0x38 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    W: 0x88 0x77 0x66 0x55 
    R: 0x00 0x00 0x00 0x00 
    W: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    W: 0x61 0x81 0xbc 0x06 
    R: 0xa0 0x00 0x00 0x00 
    W: 0x04 0x8c 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    W: 0x00 0x3a 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    W: 0x44 0x33 0x22 0x11 
    R: 0x00 0x00 0x00 0x00 
    W: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    W: 0x00 0x00 0x01 0x23 
    R: 0x00 0x00 0x00 0x00 
    W: 0x00 0x00 0x00 0x3a 
    R: 0x00 0x00 0x00 0x00 
    
    Read TX BUFFER start 0x8174: 
    W: 0x41 0x81 0x74 0x24 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x05 0x10 0x00 0x00 
    R: 0x00 0x38 0x00 0x00 
    R: 0x88 0x77 0x66 0x55 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x04 0x8c 0x00 0x00 
    R: 0x00 0x3a 0x00 0x00 
    R: 0x44 0x33 0x22 0x11 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x01 0x23 
    R: 0x00 0x00 0x00 0x3a 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    
    Read TX BUFFER end 
    W: 0x61 0x10 0xd0 0x01 0x00 0x00 0x00 0x02 
    R: 0xa0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    W: 0x61 0x10 0xd0 0x01 0x00 0x00 0x00 0x01 
    R: 0xa0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    

  • HI Leon,

    I will review your register configuration information and then follow up with you on any additional questions and suggestions I have.

    Regards,

    Jonathan

  • Hi Leon,

    Sorry for the delay, but I have reviewed your register configuration. 

    I noticed that you are setting the Transmit Delay Compensation Offset (TDCO) to 0xE but the Transmit Delay Compensation Filter (TDCF) to 0x0. 

    Generally it is good to always set TDCO and TDCF to the same value.  The TDCF value sets the minimum Secondary Sample Position (SSP) in the CAN FD bit and if this value is to low, the SSP will not be correctly set by the TDCO position and this could result in bit errors.

    It looks like you are transmitting messages and the voltage levels look correct for CANH and CANL.  The portion of signals you are sharing look consistent with a lot of consecutive data bits that require periodic Stuff bits to be added.  But there is not enough of the signal for me to determine exactly what portion of the CAN message I'm looking at.

    I decode your register configuration for a Nominal data rate of 500kbps and a Data rate of 2Mbps.  Is that your intention?  Do you see a faster bit rate during your message transmission?

    I've looked back through the thread and I am unclear about what issue we are trying to resolve.  Was your question simply related to why the CANERR bit was getting set, or are there other issues preventing you from transmitting and receiving messages? 

    Can you please restate the specific issues that need to be resolved?

    Thanks,

    Jonathan

  • Hi, Jonathan.

    "I decode your register configuration for a Nominal data rate of 500kbps and a Data rate of 2Mbps.  Is that your intention?"

    yes, that is my intention, I want to configuration for a Nominal data rate of 500kbps and a Data rate of 2Mbps. 

    My main problem is that I want my code to run on the development board to achieve CAN message  transmission and receive. 

    The issue now is that I configured the hardware and write Tx buffer according to TCAN demo code, but the messages sent to the bus always have strong CNA errors. I don`t know where the problem lies.

     

    I noticed that you are setting the Transmit Delay Compensation Offset (TDCO) to 0xE but the Transmit Delay Compensation Filter (TDCF) to 0x0. 

    after I set DCO and TDCF to the same value, CANOE test had stuff error.

    I sent message according to TCAN demo code, but capture the CANH and CANL waveforms are strange. Most of them are 1(recessive). 

    I don't quite know what to do next.

    Regards,

    Leon

     

  • Hi Leon,

    Thank you, I have a better understanding now of the overall issue.  I'll point out two additional documents that are helpful that you may or may not have already seen.

    TCAN45xx Software User's Guide

    MCAN User's Manual

    Ok.  First, can you tell me which development board you are using?  Is it one created by TI such as TCAN4550EVM or BOOSTXL-CANFD-LIN?

    Can you verify if there is 120 ohms of termination on both sides of the CAN bus between CANH and CANL?

    after I set DCO and TDCF to the same value, CANOE test had stuff error.

    Does this mean you did not get CAN errors when you had TDCF set to 0 while TDCO = 14?  Or did you still get errors regardless of the TDCF setting?  I usually see CAN errors when they are set differently, but not when they are set to the same value.  So the reason for the errors may not be related to the TDCO/F settings.  However, this is important because if not set correctly, it will result in errors.  The MCAN User's Manual has more information on how these two settings create the Secondary Sample Point.

    Have you verified the CANoe bit timing matches the TCAN4550 configuration?  It is possible to have bit errors in CAN FD messages if the bit rates are the same, but there are different numbers of time quanta used and the sample point is in a different position in the bit period.  This is because the switch from the Nominal bit rate to the Data bit rate occurs at the sample point in the BRS bit in the message.  If the sample points are different between the nodes, then one device may switch to FD mode before another device is ready and an error is generated.  So, it is always recommended to have the same settings for all nodes on a CAN bus.

    Can you receive messages sent from CANoe without errors, or do you get errors when trying to receive messages as well?  We need to see if errors are generated for both RX and TX messages, or for only one direction so that we can find the root cause.

    Can you provide scope plots of an entire CAN message being transmitted?  Because CANH and CANL are differential, it's best to have the same GND reference location on the scope so the waveforms are aligned properly without a separation.

    Can you also monitor or log the following registers during your test so we can see specifically what interrupt, status, and Error Counter bits are getting set?

    0x0820 - Device Interrupts

    0x0824 or 0x1050 - MCAN Interrupts

    0x1018 - Control Register (monitor INIT bit)

    0x1040 - Error Counter Register (CAN transmit and receive error counters)

    0x1044 - Protocol Status Register (CAN specific status information including Error Codes)

    0x10A4 and 0x10B4 - RX FIFO 0 and RX FIFO 1 Status registers

    0x1098 and 0x109C - New Data registers (if using dedicated RX Buffers)

    0x10C4 - TX FIFO/Queue Status register

    0x10CC - TX Buffer Request Pending (to see if messages are pending transmission)

    0x10D8 - TX Buffer Add Request Transmission Occurred (to see if messages were successfully transmitted)

    Monitoring these register values during your debug will help see what bits are getting set and what is failing.  If a message gets a CAN error, then looking at the error codes can tell us what type of error it was.

    If there are too many errors, the device will between the Error Warning, Error Passive, and Bus Off states.  You can slow down this process by setting the DAR bit in the Control register to disable the Automatic Retransmission feature so that the device only tries to transmit a message once when the TX Buffer Add Request bit is set in register 0x10D0.

    Regards,

    Jonathan

  • Hi, Jonathan

    Thank you for providing theses two documents; I have reviewed them.

    after I set DCO and TDCF to the same value, CANOE test had stuff error. I mean that I still get errors when I had TDCF set to 14 while TDCO = 14, they both have a value of 14.

    Have you verified the CANoe bit timing matches the TCAN4550 configuration?

    Yes, I verified the CANoe bit timing matches the TCAN4550 configuration.

    Can you receive messages sent from CANoe without errors, or do you get errors when trying to receive messages as well?  

    I get errors when trying to receive messages as well.

    Can you provide scope plots of an entire CAN message being transmitted?

    sorry , I only have logic analysis.

    Below is the register log when I send and receive messages:

    [TCAN] TCAN4550 Test Started...
    TCAN4x5x_Device_ClearSPIERR & Disable all non-MCAN Interrupt
    If the Power On ,clear.TCAN4x5x_MCAN_EnableProtectedRegisters : 1
    GlobalFilter
    NominalTiming_Simple
    DataTiming_Simple
    MRAMConfiguration
    DisableProtectedRegisters
    Device_Configure
    Device_SetMode
    ClearInterruptsAll
    Read TX BUFFER start 0x8174: 
    Read TX BUFFER end 
    Device Interrupts 0x0820:
    W: 0x41 0x08 0x20 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    MCAN Interrupts 0824
    W: 0x41 0x08 0x24 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x0b 0x81 0x00 0x00 
    MCAN 0x1050 Interrupts
    W: 0x41 0x10 0x50 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x0b 0x81 0x00 0x00 
    Control Register 1018
    W: 0x41 0x10 0x18 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x03 0x01 
    Error Counter Register (CAN transmit and receive error counters) 1040
    W: 0x41 0x10 0x40 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x1f 0x00 0xf8 
    0x1044 - Protocol Status Register 1044
    W: 0x41 0x10 0x44 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x07 0xe5 
    RX FIFO 0 Status registers 0x10A4
    W: 0x41 0x10 0xa4 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    FIFO1 SR 0x10B4
    W: 0x41 0x10 0xb4 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    TX FIFO/Queue Status register 10C4
    W: 0x41 0x10 0xc4 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x20 0x00 0x00 
    TX Buffer Request Pending 0X10CC
    W: 0x41 0x10 0xcc 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x03 
    TX Buffer Add Request Transmission Occurred 10D8
    W: 0x41 0x10 0xd8 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    

  • when I set the DAR bit in the Control register to disable the Automatic Retransmission:

    [TCAN] TCAN4550 Test Started...
    TCAN4x5x_Device_ClearSPIERR & Disable all non-MCAN Interrupt
    If the Power On ,clear.TCAN4x5x_MCAN_EnableProtectedRegisters : 1
    GlobalFilter
    NominalTiming_Simple
    DataTiming_Simple
    MRAMConfiguration
    DisableProtectedRegisters
    Device_Configure
    Device_SetMode
    ClearInterruptsAll
    Read TX BUFFER start 0x8174: 
    Read TX BUFFER end 
    Device Interrupts 0x0820:
    W: 0x41 0x08 0x20 0x01 
    R: 0x00 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    MCAN Interrupts 0824
    W: 0x41 0x08 0x24 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x09 0x81 0x00 0x00 
    MCAN 0x1050 Interrupts
    W: 0x41 0x10 0x50 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x09 0x81 0x00 0x00 
    Control Register 1018
    W: 0x41 0x10 0x18 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x03 0x40 
    Error Counter Register (CAN transmit and receive error counters) 1040
    W: 0x41 0x10 0x40 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x12 0x00 0x90 
    0x1044 - Protocol Status Register 1044
    W: 0x41 0x10 0x44 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x07 0x6d 
    RX FIFO 0 Status registers 0x10A4
    W: 0x41 0x10 0xa4 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    FIFO1 SR 0x10B4
    W: 0x41 0x10 0xb4 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    TX FIFO/Queue Status register 10C4
    W: 0x41 0x10 0xc4 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    TX Buffer Request Pending 0X10CC
    W: 0x41 0x10 0xcc 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    TX Buffer Add Request Transmission Occurred 10D8
    W: 0x41 0x10 0xd8 0x01 
    R: 0xa0 0x00 0x00 0x00 
    R: 0x00 0x00 0x00 0x00 
    

  • Hi Leon,

    Thanks for the register data.  The PEA bit in the Interrupt register shows there is a Protocol Error in Arbitration Phase when the Nominal Bit Time is being used. 

    The Last Error Code value is 5 - Bit0Error.  During the transmission of a message (or acknowledge bit, or active error flag, or overload flag), the devcie wanted to send a dominant level (data or identifier bit logical value '0'), but the monitored bus value was recessive.

    The Transmit Error Counter is showing a lot of errors which is in turn leading to a Bus Off condition where the device removes itself from communicating on the CAN bus and sets the INIT bit in the Control register back to 1.  The first log shows a Bus Off condition which is likely from when the device repeatedly tries to transmit a message resulting in a new transmit error for each failed attempt.

    The second log is when you disabled the automatic retransmission which shows that there are transmit errors, but the not enough to enter a Bus Off condition.

    So there could be something wrong with either the Physical CAN bus such as incorrect termination, or an incorrect wiring, etc., or a potential issue with the configuration between the devices on the nodes such as different bit timing configuration etc.

    One possible issue that can create issues is the switch between the Nominal bit rate and the faster CAN FD Data bit rate.  For now, can you try to communicate without the Bit Rate Switch by setting the BRS bit in the TX Message Header to "0" so that the message will only be transmitted at the Nominal Bit Rate?  If this is error free, then the transition between the Nominal and Data bit rates is likely where the transmit error is occurring.

    Also, if you can look at the CAN message waveforms during a transmission and verify the bit times match the bit rate, the bit values match the protocol and reach the correct amplitude levels etc., or whether there is a specific bit in the message the error is occurring on, that can help us identify the cause of the error. 

    Regards,

    Jonathan