Part Number: TUSB9261
Tool/software:
I have had to swap the + and - on the super speed TX and RX signals to route cleanly, but I don't see where in the F/W I need to set to tell the chip that they are swapped.
Can you point that out?
Thanks,dan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB9261
Tool/software:
I have had to swap the + and - on the super speed TX and RX signals to route cleanly, but I don't see where in the F/W I need to set to tell the chip that they are swapped.
Can you point that out?
Thanks,dan
Hi Dan,
There is not a firmware that corrects a swap by the USB SuperSpeed Tx polarity. There is only firmware that corrects for the SATA Rx/Tx polarity swap.

It should be OK to swap the USB SuperSpeed polarity without special firmware.
Regards,
Nicholaus
Yes, Automatic Lane Polarity Inversion is included as a part of the USB 3.0 specification.
Regards,
Nicholaus
It also is mentioned in the datasheet section 10.1.2: https://www.ti.com/lit/ds/symlink/tusb9261.pd
Regards,
Nicholaus