Part Number: TMUXHS4412
Tool/software:
Hi
Some Channels of Port B is unused. Do these pins have to be pulled up or down or can they be left floating if unused ?Whether it needs to be grounded?
Regards,
Vinay
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMUXHS4412
Tool/software:
Hi
Some Channels of Port B is unused. Do these pins have to be pulled up or down or can they be left floating if unused ?Whether it needs to be grounded?
Regards,
Vinay
Hi Vinay,
Suggestion is to use AC coupling Cap plus 49.9-ohm Resistors to GND. This is done to reduce noise propagation through the device. It will be good to use 50-phm traces going to these AC coupling Cap as well. I have copied my colleague Brian since he has more experience on this part as well.
Regards, Nasser
Hi Nasser,
Please share the details on the AC caps value. It will be helpful if you can share Example schematic for the same.
Regards,
Vinay
Hi,
Whether the P and N port of each unused channel can be shorted and connected to AC Caps, Resistor?Please confirm the circuit connection for the MUX (TMUXHS4412) attached below.

Regards,
Vinay
Hi Vinay:
For unused channels, please connect to 100nf and 50 ohm to gnd.
Regards
Brian