Part Number: TCA39306
Other Parts Discussed in Thread: SN74LVC2G66, LSF0002
Tool/software:
Hi,Teams
I am considering using TCA39306 for I2C level shifting and switching.
The pull-up voltage can be adjusted to 1.2V/1.8V/3.3V, but it should be set so that V_PU1≦V_PU2.
I believe that the attached circuit should work fine if there is a voltage difference.
Would it also work if V_PU1=V_PU2?