Part Number: PCA9518
Other Parts Discussed in Thread: TCA9517A, TCA9617B
Tool/software:
Hi There,
If we are expecting 1uA of output current for the PCA 9518 below, what would be the VOL in these cases?

Thank you!
Kara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kara,
It would most likely be somewhere in the typical range (0.52V). I believe the 0.45V and 0.7V are edge cases found when sinking the max current (6mA) at cold and hot temperatures.
I would expect 0.52V in lab testing though.
Also, PCA9518 has a clock stretching errata. I highly recommend to move devices to something like the TCA9548, or try one of our single channel buffers such as the TCA9517A, TCA980x, TCA9617B. These are more reputable parts, designed with newer processes with no bugs.
Regards,
Tyler