This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUXHS4212: Why is the differential I/O specification of TMUXHS4212 -0.5~2.4V?

Part Number: TMUXHS4212

Tool/software:

Hi Team,

The USB differential signal is a 3.3V voltage level.
Why is the differential I/O specification of TMUXHS4212 -0.5~2.4V?
And the differential signal of HDMI also takes the 3.3V level.