Part Number: DP83867E
Tool/software:
Dear TI team,
I have some related questions about DP83867E's CLK_OUT signal.
1) DS states:

From that I understand that I can route CLK_OUT output of one PHY to XI of the other one. How many PHYs can be chained in this way?
2) How do CLK_OUT output behave during reset and power down?
3) If I reset e.g. the first PHY in the chain, does it stop its CLK_OUT clock, so function of other PHY is disrupted and all PHYs need to be reset too?
4) Can I safely release reset of all the PHYs in chain at once?
5) DS also states that PHY doesn't need explicit reset after power-on. Is it still true for chained PHYs?
6) All diagrams in DS show clock running before power-up. This cannot be done in chain of PHYs. I haven't found such condition in text of DS and it seems to me that in case of using crystal it is not fulfilled either. Is there any real requirement on clock being stable before power-up?
Thanks for information
Best regards
Marek