Part Number: TPD8S009
Tool/software:
Hi,
1. Can HP Detect signal in DP interface be connected to this IC?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD8S009
Tool/software:
Hi,
1. Can HP Detect signal in DP interface be connected to this IC?
Thanks
Hi Nachiketh,
I do not believe there would be any issues with using TPD8S009 on the Hot Plug Detect pin for DisplayPort. However, this device may have too large of a parasitic capacitance value if it is also being used on the TMDS channels depending on the data speed you are using. Because of this, we typically recommend TPD4E05U06DQAR or TPD4E02B04DQAR. These are both 4 channel devices, but have a much lower capacitance that allows for high speed data protection.
Please let me know if you have any additional questions!
Best Regards,
Josh Prushing