This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: part of the display image is distorted

Part Number: SN65DSI86

Tool/software:

Hi,

the color bar pattern is displayed correctly but when loading graphics (weston)

some of the image is corrupted always in the same place.

it was tested with two different displays (AUO,BOE) with a static image (weston terminal background) 

and video.

kernel version is 6.1 under NXP imx8mp yocto (langdale)

using 4 dsi lanes and 2 eDP lanes, ref clock is 27Mhz,

display is at 146500hz:

# edid-decode -c /sys/devices/pci0000:00/0000:00:02.0/drm/card0/card0-eDP-1/edid -n
edid-decode (hex):

00 ff ff ff ff ff ff 00 09 e5 fc 0a 00 00 00 00
0d 1e 01 04 95 1f 11 78 02 ef 35 95 5d 59 94 2a
21 50 54 00 00 00 01 01 01 01 01 01 01 01 01 01
01 01 01 01 01 01 3a 39 80 04 71 38 28 40 30 20
36 00 35 ae 10 00 00 1a c8 2d 80 04 71 38 28 40
30 20 36 00 35 ae 10 00 00 1a 00 00 00 fe 00 58
59 43 30 35 80 4e 56 31 34 4e 34 4e 00 00 00 00
00 00 41 21 99 00 10 00 00 0a 01 0a 20 20 00 d9

----------------

Block 0, Base EDID:
EDID Structure Version & Revision: 1.4
Vendor & Product Identification:
Manufacturer: BOE
Model: 2812
Made in: week 13 of 2020
Basic Display Parameters & Features:
Digital display
Bits per primary color channel: 6
DisplayPort interface
Maximum image size: 31 cm x 17 cm
Gamma: 2.20
Supported color formats: RGB 4:4:4
First detailed timing includes the native pixel format and preferred refresh rate
Color Characteristics:
Red : 0.5849, 0.3652
Green: 0.3505, 0.5810
Blue : 0.1640, 0.1318
White: 0.3134, 0.3291
Established Timings I & II: none
Standard Timings: none
Detailed Timing Descriptors:
DTD 1: 1920x1080 60.002 Hz 16:9 67.202 kHz 146.500 MHz (309 mm x 174 mm)
Hfront 48 Hsync 32 Hback 180 Hpol P
Vfront 3 Vsync 6 Vback 31 Vpol N
DTD 2: 1920x1080 48.001 Hz 16:9 53.761 kHz 117.200 MHz (309 mm x 174 mm)
Hfront 48 Hsync 32 Hback 180 Hpol P
Vfront 3 Vsync 6 Vback 31 Vpol N
Alphanumeric Data String: 'XYC05'

the display panel driver (panel-edp.c) timings match the edid,

thanks.