Part Number: DP83867IS
Tool/software:
Does the RGMII standard or the DP83867 guarantee that an 802.3 preamble will always begin on the rising edge of rx_clk? It's not an issue when in 10 or 100 Mb modes, but it seems that it should be case when in 1000 Mb mode. The 802.3 standard defines everything in terms of octets, so things are perfectly clear for a GMII interface. However the RGMII standard was developed outside of 802.3 and it doesn't seem to show any indication of Preamble or SFD relationship to clock edge. This seems to be an important detail since a SFD (per the 802.3 definition of 10101011) could be missed if the wrong clock edge is used to re-assemble the octet (e.g 1011xxxx).
Thanks,
John