Part Number: TPD6E004
Tool/software:
Hello Team,
I am developing a signal switching circuit for my use case with a control unit.
Please find below the supply diagram of my PCB

The shield of the USB and the Ethernet (in MSP432) is connected to the Chassis Ground and the ESD protection diodes are placed near to the connector.
The input supply is referring to DGND and also there is an isolated power supply in our circuit referring to GND_ISO.
The above shown PCB will be connected to carrier PCB also.
1. Where should the ESD diodes be placed, since this PCB will be connected to Carrier PCB.(On control PCB or Carrier PCB)
2. Any Electrostatics in the connector should be bypassed through the ESD diodes. To which ground the ESD diode has to be connected - DGND/GND_ISO or Chassis GND?
3. Since ESD diodes are connected to the same chassis ground will the isolation get affected?
Could you please support here on this queries