Part Number: TUSB4041I
Tool/software:
Hi
I would like to enable VBUS on one downstream port with up to 500mA when the upstream port is not connected.
Is it possible to configure TUSB4041I like this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB4041I
Tool/software:
Hi
I would like to enable VBUS on one downstream port with up to 500mA when the upstream port is not connected.
Is it possible to configure TUSB4041I like this?
Hi Eugene:
If the battery charging is enabled , downstream port should still support 500mA for SDP even upstream port is not connected.
Regards
Brian
Hi Brian
Thank you for your replying.
If TUSB4041I advertises DCP or CDP to peripheral devices, they may draw up to 1.5A.
However, my application has limited power thus I'd like TUSB4041I to advertise up to 500mA to peripheral devices.
Is it possible to limit advertised current capability of TUSB4041I?
Hi Eugene::
Actually, when battery charging is enabled and upstream port is not connected, it only support DCP. TUSB4041 can not control the current limit , it all depends on DP/DM negotiation.
Regards
Brian
Hi Brian
Thank you, I understand I should not enable battery charging on my application.
Is there any way to provide VBUS on Downstream port without battery charging feature when the upstream is unconnected?
Well, you can always turn Vbus switch on to supply 5V to downstream port without PWRCTLx control from hub.
Regards
Brian