Part Number: TCAN4551-Q1
Tool/software:
Dear everyone:
Recently when we recently used the chip TCAN4551, we found that the waveform was low in the middle and high on both sides. Because this part is not a terminal node, so when this component was tested separately, a 60ohm resistor was connected in parallel at the end of the cable. The terminal resistance is removed, and the wiring diagram for the test is as follows.