Part Number: TCAN1462-Q1
Tool/software:
Hi team,
Could share which parameters are mentioned in ISO 11898-2:2016, Table14? Which parameters shown in TCAN1462-Q1 datasheet are corresponding to that?
Regards,
Ochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1462-Q1
Tool/software:
Hi team,
Could share which parameters are mentioned in ISO 11898-2:2016, Table14? Which parameters shown in TCAN1462-Q1 datasheet are corresponding to that?
Regards,
Ochi
Hi Ochi-san,
Table 14 of the ISO specification lists the bit width and timing symmetry requirements for 5Mbps CAN FD operation. These parameters are covered by tBIT(BUS), tBIT(RXD), and delta tREC fields in the FD Timing Characteristics section of the TCAN1462 datasheet (Section 8.9 page 10) with the test parameter tBIT(TXD) = 200ns.
Let me know if you have any more questions.
Regards,
Eric Schott