This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Here is some questions from customer side:
Hi Gabriel,
1. Maximum level - is the maximum signal level received from a spurious frequency component in the frequency range listed. So If there is a spurious frequency <= 3.5MHz the maximum signal level is -13dBm for the SN65HVD63. The spurious frequency component is specifically not the modulation frequency used in ASIG.
2. Yes this is a value from the standard itself.
3. The SN65HVD63 is designed to meet ASIG3.0 standard. So it meets standard.
4. SN65HVD62 is ASIG2.0 - if they need ASIG3.0 they shouldn't even look at that part. Forget that part - the only option we have is the SN65HVD63 that meets ASIG3.0.
5. Don't use it - it won't be compliant with ASIG3.0. That's all - if they try to use it against our advice they take full responsibility and liability when the system fails and our support if they come to us is "they shouldn't use this part". Don't even entertain this line of thinking - they can use HVD63 or nothing we don't really support ASIG beyond those two devices and our support is limited for these devices in general.
Best,
Parker Dodson
I have further questions about the maximum level. How we test or mesuare our device real performance this this spec?
We didn't give the spurious frequency componets signal level, it menas that no matter how large the signal level (larger than 3.5Mhz signal) before the filter, our bandpass filter could make sure the output is less than -13dBm?
Gabriel,
The information is in the chart you already posted:
If gives you the spurious frequency range - we also show the spectrums in various conditions:
This is the information we have on this device bandpass filter:
Spurious frequency doesn't have an exact number - but a range because the spurious signals are just not the fundamental modulation frequency - so it includes. It includes the 4.17MHz number because this device is backwards compatible with ASIG2.0 (but you can't use ASIG2.0 with ASIG3.0 system requirements).
Best,
Parker Dodson