Part Number: THVD1550
Tool/software:
Dear Specialists,
My customer is encountering the same situation.
I shared the information and the customer has questions listed below.
I would be grateful if you could advise.
I send the file as a reference to the customer.
THVD1550 DE RE Control Timing .pdf
---<Questions>
1. The related thread is mentioned that when both DE and RE are disabled, the device goes into standby mode.
I could not find any description of standby mode in the data sheet.
If there is a related application note, please provide it.
2. It was explained that standby mode is when both DE and RE are disabled. If /RE=L (enabled) from this state, how does it behave and why does the R output become undefined?
Could you please explain the mechanism?
3.It is recommended that RE and DE be controlled to be ON at the same time.
Is it no problem to use this way in the application example of Half-Duplex Devices in Figure 28 of P22: 10.2.2 of the data sheet?
I am concerned about whether there is any problem with turning on the driver and receiver at the same time.
---
I appreciate your great help in advance.
Best regards,
Shinichi