This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953A-Q1: Possiblity of DS90UB954 recieve eDP data to CSI and DS90UB953 transport CSI data to eDP

Part Number: DS90UB953A-Q1


Tool/software:

Hi,

We have a video card integerted with Des954,Ser953 and a FPGA inside.

The FPAG will copy all CSI data from Des954 to Ser953.

We want connect the video card between a ECU with Ser983 and monitor with Des984.

Could it be feasible?

 

If Yes,

1)What mode need to be configured in Des954 and Ser953 to be compatible to eDP data?

2)Any limitaions on the data rate?

If No,

3)Any existing hardware converter can be used in this case?