This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pulsed laser driver

I am looking for a chip with the following spec for pulsed laser drive:

- Max current 2A
- Min pulse width 1 or 1.5nsec
- Max repetition Rate  20MHz
- VCC= 5V  Max =12V

MOSFETs could be  included or not.  Does anybody could help.

Thanks