Part Number: DS280DF810
Other Parts Discussed in Thread: USB2ANY, , DS250DF810
Tool/software:
Hello,
I'm working on a custom DS280DF810 eval board. Can the device SMBus interface be controlled using a USB2ANY interface adapter and SigCon Architect software?
Here are the details I've worked out so far, please let me know if there's anything I'm missing:
J4 of the USB2ANY would connect via ribbon cable to the custom eval board. The USB2ANY contains programmable 1.5k pullups on the SDA/SCL lines, which is outside the 2k-5k pullup range suggested by the DS280DF810 datasheet. So, for example, 2.7k pullups to 3.3VEXT (sourced by the USB2ANY) should be added on the SDA/SDC pins.
Based on the DS280DF810 design files I received, it appears that SigCon Architect v2.0.0.8 with DS250DF810 profile v1.0.1.5 is the right software configuration to use. Let me know if there's a newer profile compatible with SigCon v3 that I should use instead.
Thanks,
Charlie