Part Number: DP83867IR
Tool/software:
The System should be waken by WoL of the PHY DP83867IR. Therefore, I intend to use the INT/PWDN pin as interrupt to wake the system. The PHY is driven by standby supplies.
The INT/PWDN-pin is cnfigured as PWRDOWN by default. Is there a way to configure the INT/PWDN-pin to WoL-Interrupt without register access? Since the system should not only be waken but also booten over LAN, a pre configuration over register access seems not to be a solution to us. Is there a boot strap option I have not found, or is the configuration made on registers non-volatile?
Thanks in advance,
Tom