Part Number: DP83826E
Tool/software:
I would like to know if it i permissible to have only one MDI channel namely the RX +/- with pin polarity swap.
The TX +/- channel is fine. I like to always route my pairs without vias. The run is extremely short since we are using Magic Jack Ethernet Ports, aka built in magnetics.
Running at 100Base.
From page 41 of data sheeet,
9.3.13.4 Active Link Polarity Detection and Correction Swapping the wires within the twisted-pair causes polarity errors.
Wrong polarity affects 10BASE-Te connections. 100BASE-TX is immune to polarity problems because it uses MLT-3 encoding.
10BASE-Te receive block automatically detects reversed polarity
I am uncertain of this mention and if it covers 100Base-RX, I believe that it does.
Please advise on polarity pin swap on only the RX channel.
Your advice is greatly appreciated.
Sincerely,
David