This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410: About TFP 410 T.M.D.S Signal

Part Number: TFP410

Tool/software:

Could you please check the signal state of the T.M.D,S signal when the /PD signal is Not Active?

・Power ON transition period:
・During operation:

Could you please check the signal state of the T.M.D,S signal when the /PD signal is Active?
It is written as Tristate for SII164, is this the same?
・Power ON transition period:
・During operation:

Best Regards

  • Hey,

    The ~PD signal is an active low signal.

    When ~PD is set to low the device is put into a power down state where the TMDS output pins are left in a high impedance/ High-Z state. The will be the case on power up and during operation as the pins are sampled during startup.

    When the ~PD pin is left as high, the TMDS outputs will be set to the proper DVI/ HDMI terminations and common mode voltage. This will be the case on power up and operation.