This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD1400: High current consumption

Part Number: THVD1400

Tool/software:

Hi, 

I am using THVD1400 for RS485 communication between my device. 

I have the following schematics - 

5VDC+RS485.pdf

I have a current issue when I start communicating with the device. 

the datasheet mention about 1mA consumption when the device is on -

but in fact, I see other currents when I measure VCC. 

When the driver enabled, Receiver disabled - 57mA

When the driver disabled, Receiver enabled - 22mA  

When the driver disabled, Receiver disabled - 8uA  

I want to further understand why that happens because I am using battery and I can afford such currents. 

Thank you,

Michael.