Tool/software:
Hi,
I have two questions regarding the TFP410 Reference schematics.
Q1) In the reference circuit of the TFP410, 1kΩ pull-down resistors are included for the T.M.D.S signals.
However, there is no mention in the datasheet (and guidlines) about these resistors.
Which documents are recommended?
Q2) If there are no resistors, what kind of impact can be expected?
(ex how does it affect display detection on the transceiver side?)