Part Number: TRS3243E
Tool/software:
We are investigating the cause of a part failure and would like to ask you for your advice.
We have two devices that implement an RS-232 Line Driver or Receiver.
One of the devices (a third-party driver) has a cable connected and is powered on.
The other device (TRS3243ECPWR) is powered off, and we have connected the cable and turned the power on multiple times.
Performing the above operations has resulted in a part that is no longer able to communicate over RS232C and has a different TRS3243ECPWR state.
The number of parts that have failed is 3 out of 650.
The failure rate is 100%.
We will explain the condition of good and defective parts.
Resistance between pins 3(V-) and 4(VIN1) when power is off
Good parts:Around 650kohms
Defective parts:Around 100ohms
Voltage between pins 4(VIN1) and Ground when power is turned on
Good parts:Around 0V
Defective parts:Around -5V
From this phenomenon, can you infer the cause of the problem and what is happening inside the component?
Regards
Yoda