Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS320PR810: 4 x2 bus width configuration

Part Number: DS320PR810
Other Parts Discussed in Thread: DS320PR822

Tool/software:

Hi,

The 8ch DS320PR810 supports 2 x4 and greater bus width configuration but can it support 4 x2 device (using the same refclk)?

There is the DS320PR822 or course but what limits the DS320PR810 to having a support limitation of x4 bus width?

thanks

  • Hi Alan,

    The DS320PR810 and other linear redrivers are protocol agnostic devices that don't care about specific device widths or the PCIe REFCLK. From the DS320PR810's perspective, using 8 channels as two x4 links and using 8 channels as four x2 links are essentially the same - the endpoints don't even need the same REFCLK.

    Best,

    Evan Su