Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9546A: Wrong dimensions is EasyEDA? (LCSC store)

Part Number: PCA9546A

Tool/software:

i would like to use PCA9546A in SOIC-16 package (sadly no DIP is available).

It seems there are 3 SOIC-16 packages in the data sheet packaging - I assume the difference is due to different quantity, yet it is exactly the same part, correct?

So I looked in LCSC store from the EasyEDA, and got this device:

https://www.lcsc.com/product-detail/Interface---Specialized_Texas-Instruments-PCA9546ADR_C2674051.html

i noticed several differences, such as: 

Width of end pad to end pad in datasheet is: 10.63 mm, while in PCB layout it is 7.3mm

package only width (without pads) should be 7.6, while in layout: 3.0

Ami right or am i missing anything?

Does TI provide layout models for EasyEDA?

That could be very helpful, especially if these models would include static and dynamic behavioral models.

Thank you

Yigal