This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH981-Q1: DS90UH981-Q1

Part Number: DS90UH981-Q1


Tool/software:

Hi Teams,

I have a question about DS90UH981 & DS90UH984.

In both EVM board circuit design, 

-> DS90UH981 DOUT0+ & DOUT0- need to connect 0.1uF capacitors.

-> DS90UH984 RIN0+ & RIN0- also need to connect 0.1uF capacitors.

If my circuit design need to connect  DS90UH981 DOUT to DS90UH984 RIN, should I need to put both 0.1uF, or I only need to put one 0.1uF instead?

Example image as below:

 

I appreciate your help.

Johnny