Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550
Tool/software:
Hello team,
I have a question, in my application we use the Bus Wake via RXD_INT Request (BWRR) in Sleep Mode to detect CAN activity and wake up the host MCU using the nINT pin (CANINT).
The clock is sourced from the MCU using a pll, but when the core is in stop mode (after setting the TCAN4550 to sleep mode) the MCU stops clocking the TCAN4550.
Is the TCAN4550 still able to detect CAN activity and wake up the host MCU when the clock is off?