This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84: Test Pattern

Part Number: SN65DSI84

Tool/software:

Dear Madam or Sir,

i have a behavior which is not really clear to me. I have a 10,1" Display attached to the bridge. It is a display with a resolution of 1920x1200. In most cases the the display is working perfectly but in some cases the display is starting to flickering to black. The backlight voltage and display voltage are stable. It is a display with a resolution of 1920x1200. What confuses me a little is the fact that when I start the yocto with the following register settings, an image is displayed.

If I activate the test pattern it remains dark. Only when I change the register 0x10 and 0x11 from 1920 to 960 is the test pattern displayed. 

Pleas find attached also the datasheet.

OM101AEWDLT00_VER 0.1(with all black effect)_20240415.pdf

thanks Michael