Part Number: TCA9509
Other Parts Discussed in Thread: TCA9617B
Tool/software:
Hi Team,
Please share comparision table between TCA9509DGKR and TCA9617ADGKR. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ryan,
These devices are the same pinout and same package.
Major difference is that the static voltage offset is on A-side for TCA9509
For TCA9617, static voltage offset is on B-side.
| TCA9509 | TCA9617B | |
| VCCA | 0.9V to 5.5V (1) | 0.8V to VCCB |
| VCCB | 2.7V to 5.5V | 2.2V to 5.5V |
| SVO | A-side | B-side |
| VILC (A-side for TCA9509), VIL (B-side for TCA9617B) | 150 mV (typ) | VILB = 0.4V |
| Frequency | 400kHz | 1 MHz |
| IOLA | 10 uA | 30 mA |
|
IOLB |
6mA | 30 mA |
|
Buffered pF A-side |
1 mA = ~ 150Pf depending on data rate | 550pF |
|
Buffer pF B-side |
400pF | 550pF |
(1) Low-level supply voltage
The rest of the specifications are characterized according to the I2C standard for standard mode, fast mode, and fast mode+ (TCA9617B only). Things like prop delay, and other timing specs will adhere to the I2C standard.
Regards,
Tyler