Part Number: DS90UB927Q-Q1
Other Parts Discussed in Thread: DS90UB928Q
Tool/software:
Hi,
I have a question about the SCL frequency.
Customer's evaluation method
An I2C master is connected to the DS90UB927Q (SER), and remote I2C communication is being performed with a device connected to the DS90UB928Q (DES) via FPD-Link.
Question about the SCL frequency
1) The I2C-SCL frequency output from the DES is fixed at about 66kHz regardless of the input to the SER.
Is this due to the settings of the registers 0x26 (SCL High Time) and 0x27 (SCL Low Time)?
2) The default values of the above 0x26 and 0x27 registers are 0x83=131 and 0x84=132, respectively.
When calculated from this, the SCL frequency is about 76kHz, but the actual measured value was 66kHz. Why is there a difference?
3) Can the SCL frequency output from the DES be set by a method other than the above?
4) For example, if the SCL input to SER is 100 kHz, won't the output also automatically become 100 kHz?
Best regards,
Hiroshi