The AM26LS32ACD only expects RS422 signals correct? Or can RZ and TTL signals be utilized?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The AM26LS32ACD only expects RS422 signals correct? Or can RZ and TTL signals be utilized?
Thanks
David,
While it is uncommon practice, you could try biasing one receiver input to a mid supply (i.e. 2.5V) and use the othere receiver input as data input transitioning between 0V and 5V. The reson for this is, you must create a differential voltage between both inputs.
Hope this helps and let me know how it works.
Regards,
Thomas.