Part Number: DS90UB983-Q1
Tool/software:
Hi team,
There are two questions that need to be confirmed:
1. If the following connection method is used in DP mode, are there any potential risks? For example, when the DP data line between DS90UB983RTDRQ1 and SOC is relatively short, can only a 0.1uF capacitor be used?

2.The datasheet states that "DS90UB983 does not monitor the common-mode voltage of the eDP AUX terminal from the transmitter side for plug-in detection." In DP mode, the SOC monitors the voltage level of AUX. Is the purpose of monitoring the voltage to configure the drive current and balance level?
In addition, regarding HPD: Is the handshake process as described below?
In DP mode, DS90UB983 uses the LINK result of the DOUT0+/- or DOUT1+/- data line to determine whether there is a DEVICE. When there is a DEVICE, the HPD PIN is set high to notify the SOC that AUX communication can be performed;
In eDP mode, DS90UB983 uses the LINK result of the DOUT0+/- or DOUT1+/- data line to determine whether there is a DEVICE. When there is a DEVICE, if there is no HPD signal, the SOC needs to poll the DP LINK to know that there is a DEVICE and then perform AUX communication.
BR,
Comi