This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867E: I am not able to attach the TI phy and unable to see rpm in /proc/device-tree

Part Number: DP83867E

Tool/software:

I am using TI phy DP83867. I can see i am not able to attach the Phy.

we are unable to see rpm in device tree.


this structure is added in device tree, but unable to see trace it through proc

rpm_1 = "/soc@0/pci@878000000000/mrml-bridge0@1,0/rpm@1";
ethernetB0 = "/soc@0/pci@878000000000/mrml-bridge0@1,0/rpm@1/sgmii@10";
ethernetB1 = "/soc@0/pci@878000000000/mrml-bridge0@1,0/rpm@1/sgmii@11";
ethernetB2 = "/soc@0/pci@878000000000/mrml-bridge0@1,0/rpm@1/sgmii@12";
ethernetB3 = "/soc@0/pci@878000000000/mrml-bridge0@1,0/rpm@1/sgmii@13";



Thanks 
Himanshu