Tool/software:
In section 9.1.1 of the TI manual for the TCAN4550, it says:
Selecting the crystal or clock input depends upon system implementation. To support 2 and 5 Mbps CAN FD the clock in or crystal needs to have 0.5% frequency accuracy. The minimum value of 20 MHz is needed to support CAN FD with a rate of 2 Mbps. The recommended value for CLKIN or crystal is 40 MHz to meet CAN FD rates up to 5 Mbps data rates in order to support higher data throughout
We are planning on running our CAN bus no faster than 125Kbps. Can you tell me what the minimum clock frequency needs to be for running the bus at that speed (we are assuming it would be less than a 20MHz clock because we see the scaling down from 40MHz to 20MHz when dropping from 5Mbps to 2Mbps)?
Additionally, can you tell me the required frequency accuracy to support running at a rate of 125Kbps?
Thank you!
Sandra Capri