Part Number: TUSB2046B
Tool/software:
Dear Sir,
We are using TUSB2046B USB HUB in our design for 2 ports. I have followed the designing wrt what mentioned in datasheet whether it may be related to termination resistors or optional filter of 22pf. While designing, I got certain doubts which I want to clarify from your side. Doubts are listed below:
1) As it 4 port hub, we are using only 2 ports so I terminated the DM3,DM4 & DP3,DP4 of other 2 ports by a 15kohm resistors wrt ground, as shown in MSP430F5529IPN eval user guide schematic. I don't know what to do PWRON & OVRCURRENT pin?
2) As we are following MSP430F5529IPN eval kit USB hub design, in that 6Mhz crystal oscillator is used but these part is not available on any website means it is obsolette. Can we use internal 48Mhz or can you suggest other 6Mhz crystal. So, these USB HUB functions properly.
3) The reset pin of USB HUB which is active low is pulled by a 47K resistor. Can you help me out in knowing how these resistor value is selected as I want to learn. Means, if there is any current parameter which is taken in consideration while selecting this resistor. Can I use 10k resistor instead of these?
4) As our USB HUB is self powered and we are using only 2 downstream ports. In downstream ports, we are not using any type A device or USB connectors. Means, in our case downstream USB port signals are going directly to our controller USB 2.0 port and one to USB TO UART converter IC. So, sir I need to know is there any need of load switch ? As in MSP eval kit load switch is not used.
Waiting for your reply,
Regards,
Shubham